AXIS#.VL.FBFILTER
Description
This parameter returns the same value as AXIS#.VL.FB , filtered through a 10 Hz filter.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 | |
General Information
|
Type |
Read Only |
|
Units |
Depends on AXIS#.UNIT.VROTARY (pg 1) Rotary: rpm, rps, deg/s, (custom units)/s, rad/s |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
Float |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.VL.FBFILTER | 0x5011 | 0x3 | DINT | - | Velocity | RO | False |
| AXIS2.VL.FBFILTER | 0x5111 | 0x3 | DINT | - | Velocity | RO | False |